Device Control

Electric devices can be controlled manually, hydraulically, and electronically as well as remotely. Control features capture information defining trip current, trip operation, trip interval, overcurrent duration, reclosing operation, and lockout operation of devices that are used to complete, maintain, or interrupt circuits under normal and fault conditions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?