ElectricSurvey
Electric surveys are completed periodically above ground where metal pipes are located to monitor how fast they are corroding.
Subtypes: None
Associations: Drip, LeakReport, PipeExposure
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
Amperage |
text |
System rated capacity of rectifier in amps. |
Comments |
text |
User or designer comments. |
DistributionMainObjectID |
long integer |
ObjectID of associated Distribution Main. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
ServiceObjectID |
long integer |
ObjectID of associated Service GasPipe. |
SurveyDate |
date |
Date of last Electric Survey. |
SurveyDueDate |
date |
Date next Electric Survey is due to be performed. |
SurveyFrequency |
text |
Frequency of Electric Survey. |
Voltage |
long integer |
Amount of voltage output by rectifier in amps. |