Electric Complex Edge

ElectricComplexEdge contains the common attributes of primary, secondary, overhead, and underground conductors. ElectricComplexEdge is an abstract class that includes subclasses such as busbars and communication cable. These are represented as complex edge features because multiple devices can be connected along their edge. Circuits are modeled with options for feeder identifiers to support automated switching and tracing functions.

SCADA applications in distribution systems are increasing in deregulated environments. Automated switching of feeder circuits involves supervisory control to support operator control of equipment. Data acquisition gathers telemetered data from a variety of sources to increase reliability and operator productivity.

Associations: None

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

LengthSource

text

Code indicating source of length measurement; domain values include Field Measurement and Mapping System.

MeasuredLength

long integer

Length of ElectricComplexEdge.

Subtype

long integer

Code indicating subtype of ElectricComplexEdge.

WorkOrderID

text

Utility identifier of work order.

Optional Fields

   

ParentCircuitSourceID

long integer

This field contains a value that identifies the parent circuit source to the electric device. This field is required by Extended Feeder Manager.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?