Water Field Model Names

Model Name

Object

BONDEDINDICATOR

The attribute that indicates whether a feature is bonded; if it is bonded, it will not be a barrier to a cathodic protection trace; if it is not, it will be a barrier. Used by water trace solvers.

CPSYSTEMSTATUS

The attribute that indicates whether or not a feature is a barrier to a cathodic protection trace; used by water trace solvers.

EMERISOLATIONSYSSTATUS

The attribute on a feature that indicates whether or not it is a boundary on the emergency isolation system; used by water trace solvers.

ISOLATIONLEVEL

Reserved for future use.

MATERIAL

The attribute on a feature that indicates the material of a feature to determine whether it will be a barrier to a cathodic protection trace; used by water trace solvers. Values: plastic, non-plastic.

NORMALPOSITION

The attribute on a controllable device (e.g., Valve or Controllable Fitting) that indicates whether the device is open or closed; used by water trace solvers. Values: open, closed.

OPERATINGCLASSIFICATION

The attribute on a Valve that indicates whether the valve is critical; used by water trace solvers.

OPERATINGPRESSURE

The attribute on the DistributionMain feature class that indicates the operating pressure of the pipe.

PIPEDIAMETER

The attribute on a water pipe that indicates its diameter.

PIPETYPE

The attribute on a water pipe that indicates whether the pipe is a pinchable type; used by water trace solvers. Values: pinchable, non-pinchable.

PIPESTATUSINDICATOR

The attribute on a water pipe that indicates whether the pipe is pinched or damaged in some way, such that water will not flow through it; used by water trace solvers. Values: open, closed.

SOPIN

Attribute on RegulatorStation that indicates standard or system operating pressure entering station; used by water trace solvers.

SOPOUT

Attribute on RegulatorStation that indicates standard or system operating pressure leaving station; used by water trace solvers.

STATUS

Assign to the Status field on Distribution Main, Valve, Service, and Network Source features; used by water trace solvers.

VALVEUSE

Reserved for future use.

WATERPRESSURESYSTEMSTATUS

The attribute on a feature that indicates whether or not it is a boundary on the water pressure system; used by water trace solvers.

WATERSYSTEMSTATUS

The attribute on a feature that indicates whether or not it is a boundary on the water system; used by water trace solvers.

WATERTRACEWEIGHT

The attribute on all feature classes that represents the trace weight in the geometric network; used by water trace solvers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?