Underground Structure

UndergroundStructure is a simple junction feature that includes vaults and manholes that house and protect electrical equipment.

Figure 1, Transformer Vault

Subtypes: Hand Hole, Manhole, Vault. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Associations: ElectricDevice, ElectricLocation

Model Names: STRUCTURE

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

ConstructionStatus

long integer

This field contains a value from the Construction Status domain that indicates the current status of construction on the structure (e.g., proposed, existing, retired).

FacilityDiagram

text

This field contains a value from the Yes/No Indicator domain that indicates whether a facility diagram exists for the underground structure.

FacilityID

text

Meaningful company-assigned unique identifier. Uses the FACILITYID model name on this field.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

Manufacturer

text

Manufacturer of UndergroundStructure.

Material

text

Material of UndergroundStructure.

Model

text

Model of UndergroundStructure.

StructureSize

text

Size of structure.

StructureType

text

Type of UndergroundStructure.

SymbolRotation

double

Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features.

WorkOrderID

text

Utility work order identifier.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?