Strainer

Like a scrubber, this device is used to remove or “strain” foreign materials from natural gas (e.g., dirt, dust).

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

ConnectionDiameter

text

Size of connection.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

DesignPressureEntered

double

System pressure, in any unit of measure.

DesignPressureStandard

double

Derived field displaying calculated standard system pressure.

DesignPressureUnitOfMeasure

text

System pressure standard unit of measure; domain values include psi, iwc, etc.

MaxDifferentialPressure

double

Maximum differential pressure rating across strainer.

Owner

text

Owner of associated facility.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?