Generator

Generator is an alternative, third party power source feeding into the electrical network.

Associations: None

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

ConnectionConfiguration

text

Code indicating type of connection of Generator; domain values include Delta and Wye.

GroundReactance

long integer

Reactance of ground in ohms.

GroundResistance

long integer

Resistance of ground in ohms.

kW

long integer

Power rating in kW.

MaxReactiveGeneration

long integer

Maximum reactive generation.

NominalVoltage

long integer

Code indicating system voltage for which device is rated; domain values include 4.16 kV Grounded Y, 7.2 kV Grounded Y, etc.

PositiveSequenceReactance

double

Equivalent positive sequence reactance seen at source by downstream circuit in ohms.

PositiveSequenceResistance

double

Equivalent positive sequence resistance seen at source by downstream circuit in ohms.

PowerFactor

double

Power factor rating, expressed as percentage.

Rated KVA

long integer

Rated kVA.

SubtransientReactance

double

Subtransient reactance.

TransientReactance

double

Transient reactance.

ZeroSequenceReactance

double

Equivalent zero sequence reactance seen at source by downstream circuit in ohms.

ZeroSequenceResistance

double

Equivalent zero sequence resistance seen at source by downstream circuit in ohms.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?