Combo Autoupdaters

The order of simple autoupdaters called in a combo autoupdater's sequence may be important. For example, in the case of the ArcFM Split/Relate/Create Feeder Object combo autoupdater, it is important that the ArcFM Segment Split autoupdater be called before the ArcFM Internal FeederID Create autoupdater so that the tracing actions launched by the latter will be aware of the new edges introduced by the former. Autoupdaters that have Internal as part of their name are never used by themselves in the Minerville sample database. They are only used in these combo autoupdaters that support Feeder Manager.

IMPORTANT: When assigning a combo autoupdater, be sure to unassign any of its constituent autoupdaters from the same event.

Autoupdater Name

Sequence of Simple Autoupdaters

Compatibility

ArcFM Create Feeder Object

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Internal FeederID Create

Desktop

Server

ArcFM Create Squeeze Off

  1. ArcFM Check for Pinchable Pipe

    If yes, then

  2. ArcFM Segment Split

Desktop

ArcFM OH — Delete Feeder Conductor/Units

  1. ArcFM Delete Feeder Object

  2. ArcFM Delete Related Conductor Info

Desktop

Server

ArcFM Relate/Create Feeder Object

  1. ArcFM Structure Relate

  2. ArcFM Generic Electric Trace Weight

  3. ArcFM Internal FeederID Create

Desktop

Server

ArcFM Relate/Update Feeder Object

  1. ArcFM Structure Relate

  2. ArcFM Generic Electric Trace Weight

  3. ArcFM Internal FeederID Update

Desktop

Server

ArcFM Split/Create Feeder Object

  1. ArcFM Segment Split

  2. ArcFM Generic Electric Trace Weight

  3. ArcFM Internal FeederID Create

Desktop

Server

ArcFM Split/Relate Feeder Object

  1. ArcFM Segment Split

  2. ArcFM Structure Relate

Desktop

Server

ArcFM Split/Relate/Create Feeder Object

  1. ArcFM Segment Split

  2. ArcFM Structure Relate

  3. ArcFM Generic Electric Trace Weight

  4. ArcFM Internal FeederID Create

Desktop

Server

ArcFM Update XFR KVA/Synch Phase

  1. ArcFM Update Rated kVA

  2. ArcFM Synch Transformer Phase

TIP: This AU is disabled on non-subtyped transformers.

Desktop

Server

ArcFM UG — Delete Feeder Conductor/Units

  1. ArcFM Delete Feeder Object

  2. ArcFM Remove Deleted ULS Member

  3. ArcFM Delete Related Conductor Info

Desktop

ArcFM Update Feeder Object

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Internal FeederID Update

Desktop

Server

ArcFM Update UG Feeder Object

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Internal FeederID Update

  3. ArcFM Check Cross Section

Desktop

Server

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?