Electric Location

Associations: FacilityStructure, UndergroundStructure

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

ConstructionStatus

long integer

This field contains a value from the Construction Status domain that indicates the current status of construction on the structure (e.g., proposed, existing, retired).

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

ElectricTraceWeight

long integer

Used by Feeder Manager to determine device status and other information that affects circuit connectivity.

FeederID

text

Feeder Manager identifier assigned to feeders and devices that participate in a specific distribution circuit.

FeederID2

text

Feeder Manager identifier assigned if device is supplied by second feeder.

FeederInfo

long integer

Feeder Manager-assigned phase information describing the phase of the circuit that supplies a device.

InstallationDate

date

Date of installation of ElectricLocation.

LocationID

text

Utility-assigned identifier of ElectricLocation.

Subtype

long integer

Code indicating subtype.

SymbolRotation

double

Angle of rotation dictating how a feature appears on the map.

WorkOrderID

text

Work order identifier.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?