CPBondJunction
In cases where plastic pipe connects two metal pipes, bonding wire is used to maintain the electrical connectivity throughout the cathodic protection system. The CPBondJunction is a location where two to four bonding wires come together.
You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPBondJunction feature class.
CPBondJunction acquires properties from the CathodicProtectionDevice abstract class.
Subtypes: None
Associations: CPBondWire
Model Names: GASNONTRACABLE
Attributes:
Field Name |
Field Type |
Description |
BondJunctionType |
text |
Code indicating type of bond junction; examples include Above Ground, Above Ground with Foreign Line, and Curb Box Bond. |
CPBondWireObjectID |
long integer |
Object ID for bonding wire used in bond junction. |
CriticalIndicator |
text |
Code indicating whether bond wire is essential to maintain connectivity; domain values are Yes or No. |
ResistanceIndicator |
text |
Code indicating whether CPBondJunction has resistance; domain values are Yes or No. |