GasDevice
GasDevice is an abstract class. Gas devices control the flow of gas through a network of pipes, measuring and controlling the pressure at which gas is delivered. Features, including GasValve, PressureMonitoringDevice, GasLamp, ReliefValve, GasStation, and RuralTap inherit common characteristics from the GasDevice abstract class.
Subtypes: None
Associations: None
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
Comments |
text |
User or designer comments. |
EquipmentID |
text |
Utility-assigned identifier that remains with equipment if it is moved. |
FacilityID |
text |
Utility identifier representing a feature’s location in the facility; if the feature is replaced, the new feature has the same identifier. |
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
InServiceDate |
date |
Date device was installed. |
InstallationDate |
date |
Date of installation. |
Owner |
text |
Owner of GasDevice. |
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
Subtype |
long integer |
Code indicating type of GasDevice, examples include Gas Lamp, Relief Valve, and Gas Station. |
SymbolRotation |
double |
Angle that dictates how the feature appears on a map. |
WorkOrderID |
text |
Utility-assigned identifier of work order. |