Capacitor Control

Capacitors maintain or increase the voltage of distribution conductors and reduce voltage drops in the system. Subtypes include CurrentLevel, KVARLevel, TempLevel, Time, and VoltageLevel.

Associations: CapacitorBank, SeriesCapacitor

Subtypes: Current Level, KVAR Level, Temp Level, Time, Voltage Level. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Model Names: None

Attributes:

Field Name

Field Type

Description

DeactivateSaturday

text

Code indicating whether capacitor control deactivates on Saturday; domain values are Yes or No.

DeactivateSunday

text

Code indicating whether capacitor control deactivates on Sunday; domain values are Yes or No.

OnSetting

long integer

Indicates when capacitor bank is turned on.

OffSetting

long integer

Indicates when capacitor bank is turned off.

PFCorrectingEquipObjectID

long integer

ObjectID of associated PFCorrectingEquipment.

Phase

text

Code describing phases attached to capacitor bank; domain values include A, AB, AC, etc.

SCADAControlID

text

ID of SCADA control, if present.

SCADAMonitorID

text

ID of SCADA monitor, if present.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?