Gas Field Model Names
Model Name |
Object |
---|---|
AT_<Field Name> |
Any attribute on a feature class that should be transferred from the abandoned feature class (source) when a feature is abandoned; must also exist on the appropriate field of destination feature/object class. |
BONDEDINDICATOR |
The attribute that indicates whether a feature is bonded; if it is bonded, it will not be a barrier to a cathodic protection trace; if it is not, it will be a barrier. Used by gas tracing. |
CPSYSTEMSTATUS |
The attribute that indicates whether or not a feature is a barrier to a cathodic protection trace; used by gas trace solvers. |
EMERISOLATIONSYSSTATUS |
The attribute on a feature that indicates whether or not it is a boundary on the emergency isolation system; used by gas trace solvers. This model name is not currently in use, but will be used in future releases. |
GASPRESSURESYSTEMSTATUS |
The attribute on a feature that indicates whether or not it is a boundary on the gas pressure system; used by gas trace solvers. |
GASSYSTEMSTATUS |
The attribute on a feature that indicates whether or not it is a boundary on the gas system; used by gas trace solvers. |
GASTRACEWEIGHT |
The attribute on all feature classes that represents the trace weight in the geometric network; used by gas trace solvers. |
INSULATEDINDICATOR |
Assign to insulated indicator field (Controllable Fitting and Non-Controllable Fitting) for gas tracing. |
MATERIAL |
The attribute on a feature that indicates the material of a feature to determine whether it will be a barrier to a cathodic protection trace; used by gas trace solvers. |
NORMALPOSITION |
The attribute on a controllable device (e.g., Valve or Controllable Fitting) that indicates whether the device is open or closed; used by gas trace solvers. |
OPERATINGCLASSIFICATION |
The attribute on a Valve that indicates whether the valve is critical (see the Operating Classification domain for possible values); used by gas trace solvers. |
OPERATINGPRESSURE |
The attribute on the DistributionMain feature class that indicates the operating pressure of the pipe. |
PIPEDIAMETER |
The attribute on a gas pipe that indicates its diameter. |
PIPESTATUSINDICATOR |
The attribute on a gas pipe that indicates whether the pipe is pinched or damaged in some way, such that gas will not flow through it; used by gas trace solvers. |
PIPETYPE |
The attribute on a gas pipe that indicates whether the pipe is a pinchable type (see the Pipe Type domain for possible values); used by gas trace solvers. |
SOPIN |
Attribute on RegulatorStation that indicates standard or system operating pressure entering station; used by gas trace solvers. |
SOPOUT |
Attribute on RegulatorStation that indicates standard or system operating pressure leaving station; used by gas trace solvers. |
STATUS |
Assign to the Status field on Regular and Town Border Station features; used by gas trac e solvers. |