Warning Sign
WarningSign indicates the presence of electric lines, structures, or devices.
The WarningSign class inherits attributes from the Structure abstract class.
Subtypes: None
Associations: None
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
FacilityID |
text |
Meaningful company-assigned unique identifier. |
SymbolRotation |
double |
Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features. |
Directional Auto Angle Setter |
double |
Automatically rotates point features by the same angle of linear feature to which it is snapped, taking into account the direction the line was drawn (from point A to B, rather than point B to A). This autoupdater works only with networked features. |
Endpoint Auto Angle Setter |
double |
Automatically rotates point features by the same angle of linear feature to which it is snapped, but flipping 180 degrees to take into account the closest line endpoint to which the point feature is snapped. This autoupdater works only with networked features. |