Structures Overview

Structure is the abstract class that contains common characteristics, or attributes, for all electric structures involved in the distribution or transmission of electricity. The Structure class was created as a general top-level class for any type of facility structure. The subsystem structure contains nonnetwork (nonspatial) features and related objects. You can create associations between a support structure and the Inspection object class to capture information about maintenance, for example. The subsystem structure also includes objects to manage information about the life cycle of a structure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?