Feeder Manager Autoupdaters

Feeder Manager autoupdaters are special autoupdaters that support Feeder Manager functionality. To initialize several tasks concurrently, some autoupdaters are combined. Below is a list of autoupdaters that can be used with Feeder Manager 1 or Feeder Manager 2:

Component

Description

Used by Feature Classes

Visible?

Product Compatibility

ArcFM Create Feeder Object

Combo = Generic Electric Trace Weight + Internal FeederID Create

BusBar, DynamicProtectiveDevice, Fuse, Switch, OpenPoint, Transformer, PrimaryMeter, UGElectricLineSegment, OHElectricLineSegment

Yes

Desktop

Server

ArcFM Delete Feeder Object

Maintains FeederID in response to a delete event

 

Yes

Desktop

Server

ArcFM Feeder Cache Maintenance AU

Please see the ArcFM Feeder Cache Maintenance Autoupdater topic for detailed information.

     

ArcFM Generic Electric Trace Weight

Updates the trace weight field for a database. It relies on model names rather than a specific data model

 

Yes

Desktop

Server

ArcFM Internal FeederID Create

Maintains FeederID in response to a create event

 

No

Desktop

Server

ArcFM Internal FeederID Update

Maintains Feeder ID in response to an update event

 

No

Desktop

Server

ArcFM OH — Delete Feeder Conductor/Units

Combo = Delete Feeder Object + Remove Conductor Units

OHElectricLineSegment

Yes

Desktop

Server

ArcFM Relate / Create Feeder Object

Combo = Structure Relate + Create Feeder Object

 

Yes

Desktop

Server

ArcFM Relate / Update Feeder Object

Combo = Structure Relate + Update Feeder Object

 

Yes

Desktop

Server

ArcFM Split / Relate / Create Feeder Object

Combo = Segment Split + Structure Relate + Create Feeder Object

 

Yes

Desktop

Server

ArcFM Split Feeder Object

Maintains FeederID in response to a split event

UGElectricLineSegment, OHElectricLineSegment

Yes

Desktop

Server

ArcFM UG Delete Feeder Conductor/Units

Combo = Delete Feeder Object + Remove Deleted ULSMember + Remove Conductor Units

BusBar, DynamicProtectiveDevice, Fuse, Switch, OpenPoint, Transformer, PrimaryMeter, UGElectricLineSegment, OHElectricLineSegment

Yes

Desktop

Server

ArcFM Update Feeder Object

Combo = Generic Electric Trace Weight + Internal FeederID Update

BusBar, DynamicProtectiveDevice, Fuse, Switch, OpenPoint, Transformer, PrimaryMeter, UGElectricLineSegment, OHElectricLineSegment

Yes

Desktop

Server

ArcFM Update UG Feeder Object

Combo = Generic Electric Trace Weight + Internal FeederID Update + Check Cross Section

 

Yes

Desktop

Server

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?