Designer NonCreatable Features

The following feature classes are created in the Designer dataset when you use the ArcFM Solution Object Converter to convert to Designer objects. This is the only way these features may be created.

Field

Description

Design

Placed in the Designer dataset to prevent this feature class from displaying in the CUs tab.

WorkLocation

Placed in the Designer dataset to prevent this feature class from displaying on the CUs tab.

WorkRequest

Placed in the Designer dataset to prevent this feature class from displaying on the CUs tab.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?