GasFitting

GasFitting is an abstract class. A gas fitting is a mechanical device that connects two or more pipes. Fittings may connect similar types or sizes of pipe or dissimilar pipes. If they connect dissimilar pipe, they act as transition fittings.

ContollableFitting and NonControllableFitting derive attributes from the GasFitting abstract class.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

FittingDiameter

text

Size of GasFitting, domain values include 5/8”, 1”, 6”x6”, 8”x6”, 10”, etc.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InServiceDate

date

Date device was installed.

InstallationDate

date

Date of installation.

InsulatedIndicator

text

Indicates presence of insulation; domain values include Yes and No.

Manufacturer

text

Code indicating manufacturer of GasFitting; domain values include Central Fitting, duPont, Orangburg, Stockum, etc.

Material

text

The attribute on a feature that indicates the material of a feature to determine whether it will be a barrier to a cathodic protection trace; used by gas trace solvers.

Owner

text

Owner of GasFitting.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

Subtype

long integer

Code indicating type of GasFitting; domain values include Short Stop and Three-Way Tee.

SymbolRotation

double

Angle that dictates how the feature appears on a map.

WorkOrderID

text

Utility-defined identifier of work order.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?