Remove All Refreshes While Placing Template

You can set a Windows registry key to keep ArcFM from refreshing your map until after you place your templates:

  1. Open Windows Registry Editor.
  2. Browse to HKEY_CURRENT_USER\Software\Miner and Miner\ArcFM8.
  3. If there is not a Template Favorites key, create one by right-clicking the ArcFM8 folder and select New > Key.
  4. Open the Template Favorites folder. If there is not a SupressGraphics setting, create one by right-clicking the value list in Template Favorites and selecting New > DWORD (32-bit) Value.
  5. Right-click SuppressGraphics and select Modify...
  6. Change the Value data to 1. Click OK.
  7. Close the Registry Editor.

     

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?