V

Verified

The state that indicates a design has traveled through the entire design process flow. Only users with the Administrator role may view Verified designs.

Version

In geodatabases, an alternative representation of the database that has an owner, a description, a permission (private, protected, or public), and a parent version. Versions are not affected by changes occurring in other versions of the database.

Vertex

One of a set of ordered x,y coordinates that constitutes a line.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?