Control Point

ControlPoint can be used to identify specific point depths along a main.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Depth

double

Depth of ControlPoint.

InstallationDate

date

Date of installation.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

LocationDescription

text

Verbal description of location.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?