LeakRepair

LeakRepair refers to a pipe that requires, and is scheduled to receive, repair.

Subtypes: None

Associations: LeakReport

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User and designer comments.

DimensionTie1

text

Description of east–west line of feature location.

DimensionTie2

text

Description of north–south line of feature location.

FacilityType

text

Code indicating type of facility; examples include Distribution Main, Drip, and Regulator.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

LeakCause

text

Code indicating cause of leak; domain values include Construction Defect, Damage – Third Party, Material Failure, etc.

LeakReportObjectID

long integer

ObjectID of associated Leak Report.

RepairDate

date

Date leak was repaired.

WorkOrderID

text

Utility-defined identifier of work order

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?