Publish the Map Service to ArcGIS Server

ArcGIS Server is the intermediary application - between the geodatabase and the DHFC client application - that provides DHFC access to the geospatial data.

Visit the myArcFM page DHFC Supported Versions to view the compatibility matrix among client and server versions.

During your company’s implementation, you worked with Schneider Electric to create an .mxd map document to act as the publishing source for your map service. The following topics discuss the settings of that map service, which are important to understand if you ever need to re-publish the service.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?