RFCable_OverheadSpan

There are two versions of this relationship:

  • RFCable_OverheadSpan for the as-built representation.

  • RFCable_OverheadSpan_D for the in-design representation.

Almost all of the step-by-step instructions are the same for this relationship, except for adding attributes. This relationship does have attributes added in addition to the unique identifiers. The table below explains how to add the additional attribute.

RFCable_OverheadSpan, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFCable_OverheadSpan

Origin Table or Feature Class

RFCable

Destination Table or Feature Class

OverheadSpan

Relationship Type

Simple

Forward Label

OverheadSpan

Backward Label

RFCable

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Relationship Attributes

Yes, I would like to add attributes to this relationship class

Field Name: NetworkId

Data Type: Text

Length: 255

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

OverheadSpanNetworkId

RFCable_OverheadSpan_D, the In-Design Relationship

Relationship Class Property

Value or Choice

Name

RFCable_OverheadSpan_D

Origin Table or Feature Class

RFCable_D

Destination Table or Feature Class

OverheadSpan

Relationship Type

Simple

Forward Label

OverheadSpan

Backward Label

RFCable_D

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Relationship Attributes

Yes, I would like to add attributes to this relationship class

Field Name: NetworkId

Data Type: Text

Length: 255

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

OverheadSpanNetworkId

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?