Power Supplies

Power supplies in a cable system receive power from the utility, process the power for use in the cable system, and insert it into the coaxial plant through a power inserter.

Power Supplies Details

Power Supplies

Manufacturer

The manufacturer of the component.

Model Number (required)

The component's model number. The model number is required to be unique across all resources of the same type.

Company ID

The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.

Description

A short description of the component.

GIS Symbology

GIS Symbology provides you with the ability to specify symbology text for various component specifications in Catalog. This text is published to GIS with DHFC features and can be used as a basis for symbology.

Catalog Id

The GUID assigned to the component.

Is Deprecated (default: not selected)

Toggle to mark the component as deprecated.

Power Supplies Properties

Power Supplies

Point Size (required): Assign a point value to a component based on physical size. With a consistent point value system you will be able to determine how much equipment can fit inside an enclosure. For example, if you have a pedestal rated to hold 30 points worth of components, then you can situate three 2-port taps rated at 10 points each into the box. A fourth 2-port tap would total 40 points, exceeding the rated 30 points of the pedestal.

Voltage (required)

The amount of potential energy between two points on a circuit.

Amperage (required)

The amount of electrical charge (current) that flows through a conductor in a given time.

Maximum Load Percentage (required)

Maximum load in percentage.

Number of Batteries

The number of batteries that the power supply contains, if applicable.

Is Status Monitoring

A checkbox to denote that the power supply is performing status monitoring.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?