RFNode_RFNodeCoaxPort

There are two versions of this relationship:

  • RFNode_RFNodeCoaxPort for the as-built representation.

  • RFNode_RFNodeCoaxPort_D for the in-design representation.

For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.

RFNode_RFNodeCoaxPort, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFNode_RFNodeCoaxPort

Origin Table or Feature Class

RFNode

Destination Table or Feature Class

RFNodeCoaxPort

Relationship Type

Simple

Forward Label

RFNodeCoaxPort

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriBuiltName entry in the Schema.xml file for this component.

Backward Label

RFNode

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class

Primary Key

NetworkId

Foreign Key

NodeId

RFNode_RFNodeCoaxPort_D, the In-Design Relationship

Relationship Class Property

Value or Choice

Name

RFNode_RFNodeCoaxPort_D

Origin Table or Feature Class

RFNode_D

Destination Table or Feature Class

RFNodeCoaxPort_D

Relationship Type

Simple

Forward Label

SECom.ARCFM.RFNodeCoaxPort

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriDesignName entry in the Schema.xml file for this component.

Backward Label

SECom.ARCFM.RFNode

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class

Primary Key

NetworkId

Foreign Key

NodeId

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?