Underground Structures
The Underground Structures subtab allows you to add, delete, or edit underground structures.
Existing Underground Structures
Click an existing underground structure to view its attributes. You can also utilize the filter to find the appropriate underground structure. The filter field searches the underground structure names.
After locating the underground structure, you can perform the following actions:
-
Edit: Make changes to the underground structure Name, then click Save.
-
Copy: This copies the current underground structure and then awaits edits. After you click Copy, the application appends the word “(copy)” to the Name. Then, make edits as needed and Save. If you do not make edits and Save, the copied underground structure is discarded.
-
Delete: This deletes the current underground structure. After you click Delete, click Yes to confirm or No to stop the delete process. If you click Yes, there is no undo for deleting an underground structure.
New Underground Structures
Click the Add New icon to get started.
-
Fill in the Identification field:
-
Name: Name of the underground structure.
-
-
Click Save.