UndergroundSpan_Duct

Because there is no in-design representation of UndergroundSpan or Duct, there is only one version of this relationship:

  • UndergroundSpan_Duct for the as-built representation.

For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.

UndergroundSpan_Duct, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

UndergroundSpan_Duct

Origin Table or Feature Class

UndergroundSpan

Destination Table or Feature Class

Duct

Relationship Type

Simple

Forward Label

Duct

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriBuiltName entry in the Schema.xml file for this component.

Backward Label

UndergroundSpan

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class

Primary Key

NetworkId

Foreign Key

UndergroundSpanId

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?