Amplifier Internal Equalizers

Amplifier internal equalizers reverse the non-linear attenuation of frequencies that the coaxial path causes, attenuating only the low-band to restore a degree of linearity or positive slope between hyper and low band frequencies.

Amplifier Internal Equalizers Details

Amplifier Internal Equalizer

Manufacturer

The manufacturer of the component.

Model Number (required)

The component's model number. The model number is required to be unique across all resources of the same type.

Company ID

The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.

Description

A short description of the component.

Catalog Id

The GUID assigned to the component.

Is Deprecated (default: not selected)

Toggle to mark the component as deprecated.

Amplifier Internal Equalizers Properties

Amplifier Internal Equalizers.

Equalizer Value in dB (required)

The auto-optimization engine uses this value in calculations for optimizing your network design in Designer HFC.

Equalizer Type (required)

Select Forward or Return from the drop-down list.

Insertion Loss (required)

Loss of signal strength at the insertion point.

  • Remove: Click the Remove button to the right of the value that you want to delete.

  • Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.

  • Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?