Mapping
The Mapping tab facilities the underlying basemap capabilities of the DHFC application.
There are four subtabs:
-
Feature Service: This is the URL for your published map service. This URL points to the feature service that has editing capabilities enabled for the DHFC layers.
-
Reference Maps: These map services provide reference data to the DHFC application in the form of non-editable graphical information such as stranding, boundaries, or other helpful GIS information that can aid the designers. After adding a Reference Map URL, use the Reference Views tabs to fine tune which layers from that map are visible and in what order.
-
Reference Views: These allow you to take a Reference Map service and then pick and choose which layers are visible and in what order. Views can comprise layers from multiple Reference Maps.
-
Basemaps: These are additional basemaps available to the DHFC application.