Configure the Geodatabase

As stated in the Perform Solution Center Configurations topic, an early procedure in the process is to ensure your geodatabase is ready to support DHFC. Thus, although this is “Step 4,” you will likely be doing a bulk of this work in parallel with finishing your equipment catalog in Solution Center.

The underlying geodatabase must contain certain feature classes, tables, and relationships, along with sets of required fields and properties. The following topics list these requirements starting with feature classes, then tables, and finally relationships.

To view and assign the DHFC autoupdaters, you need to install the ArcFM tools for DHFC. For the latest installers, visit the myArcFM page DHFC Installers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?