RFCable_UndergroundSpan

There are two versions of this relationship:

  • RFCable_UndergroundSpan for the as-built representation.

  • RFCable_UndergroundSpan_D for the in-design representation.

Almost all of the step-by-step instructions are the same for this relationship, except for adding attributes. This relationship does have attributes added in addition to the unique identifiers. The table below explains how to add the additional attribute.

RFCable_UndergroundSpan, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFCable_UndergroundSpan

Origin Table or Feature Class

RFCable

Destination Table or Feature Class

UndergroundSpan

Relationship Type

Simple

Forward Label

UndergroundSpan

Backward Label

RFCable

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Relationship Attributes

Yes, I would like to add attributes to this relationship class

Field Name: NetworkId

Data Type: Text

Length: 255

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

UndergroundSpanNetworkId

RFCable_UndergroundSpan_D, the In-Design Relationship

Relationship Class Property

Value or Choice

Name

RFCable_UndergroundSpan_D

Origin Table or Feature Class

RFCable_D

Destination Table or Feature Class

UndergroundSpan

Relationship Type

Simple

Forward Label

UndergroundSpan

Backward Label

RFCable_D

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Relationship Attributes

Yes, I would like to add attributes to this relationship class

Field Name: NetworkId

Data Type: Text

Length: 255

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

UndergroundSpanNetworkId

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?