RFPowerSupplyBoundary_RFPowerSupply

There are two versions of this relationship:

  • RFPowerSupplyBoundary_RFPowerSupply for the as-built representation.

  • RFPowerSupplyBoundary_RFPowerSupply_D for the in-design representation.

Almost all of the step-by-step instructions are the same for this relationship, except for adding attributes. This relationship does have attributes added in addition to the unique identifiers. The table below explains how to add the additional attribute.

RFPowerSupplyBoundary_RFPowerSupply, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFPowerSupplyBoundary_RFPowerSupply

Origin Table or Feature Class

RFPowerSupplyBoundary

Destination Table or Feature Class

RFPowerSupply

Relationship Type

Simple

Forward Label

RFPowerSupply

Backward Label

RFPowerSupplyBoundary

Message Direction

None (no messages propagated)

Cardinality

1–1 (one to one)

Relationship Attributes

Yes, I would like to add attributes to this relationship class

Field Name: NetworkId

Data Type: Text

Length: 255

Origin Primary Key

NetworkId

Origin Foreign Key

PowerSupplyBoundaryId

Destination Primary Key

NetworkId

Destination Foreign Key

PowerSupplyId

RFPowerSupplyBoundary_RFPowerSupply_D, the In-Design Relationship

Relationship Class Property

Value or Choice

Name

RFPowerSupplyBoundary_RFPowerSupply_D

Origin Table or Feature Class

RFPowerSupplyBoundary_D

Destination Table or Feature Class

RFPowerSupply_D

Relationship Type

Simple

Forward Label

RFPowerSupply

Backward Label

RFPowerSupplyBoundary

Message Direction

None (no messages propagated)

Cardinality

1–1 (one to one)

Relationship Attributes

Yes, I would like to add attributes to this relationship class

Field Name: NetworkId

Data Type: Text

Length: 255

Origin Primary Key

NetworkId

Origin Foreign Key

PowerSupplyBoundaryId

Destination Primary Key

NetworkId

Destination Foreign Key

PowerSupplyId

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?