Amplifier Internal Pads

Amplifier internal pads are plug-in attenuators that reduce input levels to a device-specific level in order to achieve desired amplifier gain with minimal distortion.

Amplifier Internal Pads Details

Amp Internal Pads

Manufacturer

The manufacturer of the component.

Model Number (required)

The component's model number. The model number is required to be unique across all resources of the same type.

Company ID

The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.

Description

A short description of the component.

Catalog Id

The GUID assigned to the component.

Is Deprecated (default: not selected)

Toggle to mark the component as deprecated.

Amplifier Internal Pads Properties

Amp Internal Pads

Pad Value in dB (required)

The auto-optimization engine uses this value in calculations for optimizing your network design in Designer HFC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?