High Tap Value Plugin

A high tap value plugin is a part of a Conditioning Tap. It is commonly used to overcome loss associated with high tap values in a cable, as part of an overall strategy to compensate for tilt.

High Tap Value Plugin Identification

High Tap Value Plugin (HT)

Manufacturer

The manufacturer of the component.

Model Number (required)

The component's model number. The model number is required to be unique across all resources of the same type.

Company ID

The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.

Description

A short description of the component.

Catalog Id

The GUID assigned to the component.

Is Deprecated (default: not selected)

Toggle to mark the component as deprecated.

High Tap Value Plugin Properties

High Tap Value

Equalizer Value in dB (required)

The auto-optimization engine uses this value in calculations for optimizing your network design in Designer HFC.

Forward Loss (required): The amount of forward signal loss at a particular frequency.

Return Loss (required): The amount of return signal loss at a particular frequency.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?