Autoupdaters

Much like any ArcFM implementation, DHFC employs Autoupdaters to perform data maintenance tasks while users are editing features. This topic describes the autoupdaters, organized by dataset.

Coax Dataset_D

There are no autoupdaters applied to any features or relationships in this dataset.

Fiber Dataset

The polygon feature classes require the autoupdater CreateCoaxNetworkId on the NetworkId fields. DHFC requires a GUID in this field, and the autoupdater assigns one when the feature is created.

Feature Class Name

Field Name

Editing Event

Autoupdater

DoNotBuildBoundary

NetworkId

On Create

CreateCoaxNetworkId

RFNodeBoundary

NetworkId

On Create

CreateCoaxNetworkId

RFPowerSupplyBoundary

NetworkId

On Create

CreateCoaxNetworkId

Landbase Dataset

There are no autoupdaters applied to any features or relationships in this dataset.

Structures Dataset

Any structure feature class (points, lines, and polygons) participating in the DHFC application requires the autoupdater CreateCoaxNetworkId on the NetworkId fields. DHFC requires a GUID in this field, and the autoupdater assigns one when the feature is created.

Feature Class Name

Field Name

Editing Event

Autoupdater

AddressPoint

NetworkId

On Create

CreateCoaxNetworkId

DownGuy

NetworkId

On Create

CreateCoaxNetworkId

MduBoundary

NetworkId

On Create

CreateCoaxNetworkId

MduPathElement

NetworkId

On Create

CreateCoaxNetworkId

MduPolygonElement

NetworkId

On Create

CreateCoaxNetworkId

MduTextElement

NetworkId

On Create

CreateCoaxNetworkId

OverheadSpan

NetworkId

On Create

CreateCoaxNetworkId

RFDrop

NetworkId

On Create

CreateCoaxNetworkId

SupportStructure

NetworkId

On Create

CreateCoaxNetworkId

UndergroundJunction

NetworkId

On Create

CreateCoaxNetworkId

UndergroundSpan

NetworkId

On Create

CreateCoaxNetworkId

UndergroundStructure

NetworkId

On Create

CreateCoaxNetworkId

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?