RFPowerInserter_RFPowerInserterPort
There are two versions of this relationship:
-
RFPowerInserter_RFPowerInserterPort for the as-built representation.
-
RFPowerInserter_RFPowerInserterPort_D for the in-design representation.
For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.
RFPowerInserter_RFPowerInserterPort, the As-Built Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFPowerInserter_RFPowerInserterPort |
Origin Table or Feature Class |
RFPowerInserter |
Destination Table or Feature Class |
RFPowerInserterPort |
Relationship Type |
Simple |
Forward Label |
RFPowerInserterPort
IMPORTANT: The Forward Label
you type while creating the relationship must match the EsriBuiltName
entry in the Schema.xml file for this component.
|
Backward Label |
RFPowerInserter |
Message Direction |
None (no messages propagated) |
Cardinality |
1–M (one to many) |
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
Primary Key |
NetworkId |
Foreign Key |
PowerInserterId |
RFPowerInserter_RFPowerInserterPort _D, the In-Design Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFPowerInserter_RFPowerInserterPort_D |
Origin Table or Feature Class |
RFPowerInserter_D |
Destination Table or Feature Class |
RFPowerInserterPort_D |
Relationship Type |
Simple |
Forward Label |
SECom.ARCFM.RFPowerInserterPort
IMPORTANT: The
Forward Label you type while creating the relationship must match
the EsriDesignName entry in the Schema.xml file for this component.
|
Backward Label |
SECom.ARCFM.RFPowerInserter |
Message Direction |
None (no messages propagated) |
Cardinality |
1–M (one to many) |
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
Primary Key |
NetworkId |
Foreign Key |
PowerInserterId |