General

The General tab provides configurations that affect functionality in the DHFC client application. These settings include:

  • Component layout offsets.

  • Which components generate tombstones.

  • Unit of measure, either Standard (US) or Metric.

  • Cable length calculation factors to account for additional cable length in aerial or underground risers.

  • Address Search default country to enhance the user experience when using the Address Search Tab.

Always click Save after making any changes. Changes are seen in the DHFC client application the next time a user logs in.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?