Tap Auto Optimize

You can specify which taps are enabled or disabled for auto optimization in the Grouping Components dialog.

After adding taps to a grouping, click the auto optimization icon to toggle on or off:

  • Auto optimization is enabled

  • Auto optimization is disabled

By default, auto optimization is enabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?