Schema

The schema.xml file provides a mapping between the ArcGIS feature service and the DHFC application objects. See the Schema.xml Configuration File help topic for more information about the file itself. The Solution Center Schema tab is for uploading the file once it is complete.

On the Schema tab, you can download the current schema file and upload the schema file after editing it.

IMPORTANT: The schema file must be a properly formatted .xml file in the structure outlined in the Schema.xml Configuration File help topic. Schema changes are immediately available to the DHFC client application. Always backup your current file prior to uploading a new one. Uploading a file overwrites the entire contents of the current schema file.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?