RFCable_Duct
There are two versions of this relationship:
-
RFCable_Duct for the as-built representation.
-
RFCable_Duct_D for the in-design representation.
Almost all of the step-by-step instructions are the same for this relationship, except for adding attributes. This relationship does have attributes added in addition to the unique identifiers. The table below explains how to add the additional attribute.
RFCable_Duct, the As-Built Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFCable_Duct |
Origin Table or Feature Class |
RFCable |
Destination Table or Feature Class |
Duct |
Relationship Type |
Simple |
Forward Label |
Duct |
Backward Label |
RFCable |
Message Direction |
None (no messages propagated) |
Cardinality |
M-N (many to many) |
Relationship Attributes |
Yes, I would like to add attributes to this relationship class |
Field Name: NetworkId |
|
Data Type: Text |
|
Length: 255 |
|
Origin Primary Key |
NetworkId |
Origin Foreign Key |
RFCableId |
Destination Primary Key |
NetworkId |
Destination Foreign Key |
DuctId |
RFCable_Duct_D, the In-Design Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFCable_Duct_D |
Origin Table or Feature Class |
RFCable_D |
Destination Table or Feature Class |
Duct |
Relationship Type |
Simple |
Forward Label |
Duct |
Backward Label |
RFCable_D |
Message Direction |
None (no messages propagated) |
Cardinality |
M-N (many to many) |
Relationship Attributes |
Yes, I would like to add attributes to this relationship class |
Field Name: NetworkId |
|
Data Type: Text |
|
Length: 255 |
|
Origin Primary Key |
NetworkId |
Origin Foreign Key |
RFCableId |
Destination Primary Key |
NetworkId |
Destination Foreign Key |
DuctId |