RFEqualizer_RFAmplifier_Fwd
There are two versions of this relationship:
-
RFEqualizer_RFAmplifier_Fwd for the as-built representation.
-
RFEqualizer_RFAmplifier_Fwd_D for the in-design representation.
For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.
RFEqualizer_RFAmplifier_Fwd, the As-Built Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFEqualizer_RFAmplifier_Fwd |
Origin Table or Feature Class |
RFEqualizer |
Destination Table or Feature Class |
RFAmplifier |
Relationship Type |
Simple |
Forward Label |
RFAmplifier |
Backward Label |
RFEqualizer |
Message Direction |
None (no messages propagated) |
Cardinality |
1–M (one to many) |
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
Primary Key |
NetworkId |
Foreign Key |
ForwardEqId |
RFEqualizer_RFAmplifier_Fwd_D, the In-Design Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFEqualizer_RFAmplifier_Fwd_D |
Origin Table or Feature Class |
RFEqualizer_D |
Destination Table or Feature Class |
RFAmplifier_D |
Relationship Type |
Simple |
Forward Label |
SECom.ARCFM.RFAmplifier |
Backward Label |
SECom.ARCFM.RFEqualizer |
Message Direction |
None (no messages propagated) |
Cardinality |
1–M (one to many) |
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
Primary Key |
NetworkId |
Foreign Key |
ForwardEqId |