RFNode_RFNodeBoundary
There are two versions of this relationship:
-
RFNode_RFNodeBoundary for the as-built representation.
-
RFNode_RFNodeBoundary_D for the in-design representation.
For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.
RFNode_RFNodeBoundary, the As-Built Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFNode_RFNodeBoundary |
Origin Table or Feature Class |
RFNode |
Destination Table or Feature Class |
RFNodeBoundary |
Relationship Type |
Simple |
Forward Label |
RFNodeBoundary
IMPORTANT: The Forward Label you
type while creating the relationship must match the EsriBuiltName
entry in the Schema.xml file for this component.
|
Backward Label |
RFNode |
Message Direction |
None (no messages propagated) |
Cardinality |
1–1 (one to one) |
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
Primary Key |
NetworkId |
Foreign Key |
NodeNetworkId |
RFNode_RFNodeBoundary_D, the In-Design Relationship
Relationship Class Property |
Value or Choice |
---|---|
Name |
RFNode_RFNodeBoundary_D |
Origin Table or Feature Class |
RFNode_D |
Destination Table or Feature Class |
RFNodeBoundary_D |
Relationship Type |
Simple |
Forward Label |
SECom.ARCFM.RFNodeBoundary
IMPORTANT: The Forward
Label you type while creating the relationship must match the EsriDesignName
entry in the Schema.xml file for this component.
|
Backward Label |
SECom.ARCFM.RFNode |
Message Direction |
None (no messages propagated) |
Cardinality |
1–1 (one to one) |
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
Primary Key |
NetworkId |
Foreign Key |
NodeNetworkId |