Conduit

Conduit helps protect and efficiently rout cables in a telecommunications network.

Conduit Details

Conduit

Name (required)

The name of the miscellaneous component.

Company ID

The ID your company assigns to the component.

Description

A short description of the component.

Catalog Id

The GUID assigned to the component.

Is Deprecated (default: not selected)

Toggle to mark the component as deprecated.

Conduit Properties

Conduit

Material (required)

Select Steel, PVC, or PE from the drop-down list.

Diameter  (required)

The diameter of the conduit. Additionally, select Inch or Millimeter from the secondary drop-down list.

Number of Ducts

Type the number of ducts that are present for the conduit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?