Reports

The reports tab lets you configure specific cable, splice, trace, and circuit stylesheet parameters for individualized reports. These settings must be saved for report generation to work correctly.

To set up your report format:

  1. Log in to Solution Center and click on the Fiber Manager plugin.

  2. On the Feature Services tab, select the applicable map from the list.

  3. On the left side menu, click the Reports tab.

  4. Next to Splice Report Format, click HTML, CSV, or XML. Next to Report Style Sheets, select a matching style sheet and click Save. Example: If you click the CSV format for the splice report format, select the splice report CSV XSL style sheet.

  5. Repeat Step 4 for the Trace, Cable, and Circuit Trace report formats and click Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?