EIO0000005081.01

Certifications and Standards

The certifications and standards listed below may include those that are not yet acquired. Please check the product marking and the following URL for the latest acquisition status.

www.se.com/ww/en/download

Agency Certifications

  • Underwriters Laboratories Inc., UL 61010-2-201 and CSA C22.2 N°61010-2-201, for Industrial Control Equipment used in Ordinary Locations

  • Underwriters Laboratories Inc., UL 121201 and CSA C22.2 N°213, for Industrial Control Equipment used in Class I, Division 2 Hazardous (Classified) Locations

  • EAC certification(Russia, Belarus, Kazakhstan)

  • IECEx / ATEX for use in zone 2 gas/ zone 22 dust

  • DNV

Compliance Standards

Europe:

CE

  • Directive 2014/30/EU (EMC)

  • Directive 2014/34/EU (ATEX)

UKCA

  • Regulation SI 2016 No.1091

  • Regulation SI 2016 No.1107

Australia:

  • RCM

Hazardous Substances

This product is designed to be compliant with the following environmental regulations, even if the product may not fall directly in the scope of the regulation:

  • RoHS, Directive 2011/65/EU and 2015/863/EU

  • RoHS China, Standard GB/T 26572

  • REACH regulation EC 1907/2006

End of Life (WEEE)

The product contains electronic boards. It must be disposed of in specific treatment channels. The product contains cells and/or storage batteries which must be collected and processed separately when they have run out and at the end of product life (Directive 2012/19/EU).

Refer to Maintenance when extracting cells and batteries from the product. These batteries do not contain a weight percentage of heavy metals over the threshold notified by European Battery Regulation 2023/1542.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.