EIO0000005081.01

Touch Panel

 

12-inch, 15-inch

10-inch Wide, 12-inch Wide, 15-inch Wide, 19-inch Wide, 22-inch Wide

Touch panel type

Resistive film (analog)

Projected capacitive

Touch points

Multi-touch (two-point touch)

Multi-touch (two-point touch)

Touch panel service life

1 million times or more

50 million times or more

Touch panel resolution

1024 x 1024

2048 x 2048

Touch mode

Not applicable

Standard mode, water detection mode, glove mode

NOTE: For details, refer to Touch Mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.