EIO0000005081.01

Introduction

The installation gasket provides protection against dust and moisture. The gasket must be inserted correctly into the groove for moisture resistance for the Panel Type.

NOTICE
GASKET AGING
  • Inspect the gasket periodically as required by your operating environment.
  • Replace the gasket at least once a year, or as soon as scratches or dirt become visible.
Failure to follow these instructions can result in equipment damage.
NOTICE
EQUIPMENT DAMAGE
Be careful not to stretch the gasket unnecessarily.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.