EIO0000005081.01

Interfaces

NOTE: Use only the SELV (Safety Extra-Low Voltage) circuit to connect all the interfaces.

Box Module

Serial interface COM

Asynchronous transmission

RS-232C/422/485 (non-isolated) x 2

(default: RS-485)

Data length

7 or 8 bits

Stop bit

1 or 2 bits

Parity

None, odd or even

Flow control

Hardware flow control: RTS/CTS(RS-232C), ERA/EAB/CSA/CSB(RS-422 HMI mode)*3

Software flow control: Xon/Xoff

Auto direction control

Always enabled only in RS-485

Echo cancellation

Supported only in RS-485*3

Data transmission speed

2,400...115,200 bps

Connector

D-Sub 9–pin (plug)

USB (Type A) interface

Connector

USB 3.1 Gen1 (Type A) x 2

Power supply voltage

5 Vdc ±5%

Maximum current supplied

900 mA/port

Maximum transmission distance

3 m (9.84 ft)

USB (Type C) interface*1

Connector

USB 3.1 Gen1 (Type C) x 1

Power supply voltage

5 Vdc ±5%

Maximum current supplied

1.5 A/port

Maximum transmission distance

3 m (9.84 ft)

Resolution

Up to 4,096 x 2,304 pixels at 60 Hz

Ethernet interface

Standard

IEEE1588, 10 BASE-T/ 100 BASE-TX/ 1000BASE-T, Wake-on-LAN (WOL) supported*2

Connector

Modular jack (RJ-45) x 2

SD card interface

SD card slot (storage) x 1

SDXC UHS-I supported

DisplayPort

Version

V 1.2, dual mode (DP++) supported

Resolution

Up to 4,096 x 2,304 pixels at 60 Hz

*1 The USB (Type C) interface supports alternate mode (DisplayPort).

*2 When the status is S4 (hybrid shutdown), Wake-on-LAN is unavailable.

*3 Echo cancellation of the serial interfaces on Box Module is set not to receive the echo (Enabled) as default. For the setting, refer to Settings of Serial Interfaces on Box Module.

Display Module

 

12-inch / 15-inch

USB (Type A) interface

Connector

USB 2.0 (Type A) x 1

Power supply voltage

5 Vdc ±5%

Maximum current supplied

500 mA

Maximum transmission distance

5 m (16.4 ft)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.