EIO0000005081.01

Model Names

Box Module and Panel Type are referred to as follows.

Panel Type is an all-in-one model in which the Box Module and Display Module are already connected.

  Box Module Panel Type
Atom Basic Box ●●-inch/●●-inch Wide Basic Model
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.